AnsweredAssumed Answered

Question about AD9106

Question asked by DanielS89 on Sep 21, 2015
Latest reply on Oct 22, 2015 by larrywelchusa

Hi all,

 

I am using the AD9106 Evaluation Board and I need some help.

 

My problem is:

 

I want to know if it is possible to use the RAM as a type of buffer,

that means I wanna set data there (e.g. samples for a waveform or values of a constant output)

and I want to Increment the RAM adress externaly or with a very low frequency.

 

Is this possible? or do I need to write the constant values via SPI with a PIC or something?

Because in the quick guide it is mentioned that i can sue the DAC-Clock or the DDS MSB

(but only for TW).

 

 

I hope someone can help me.

 

Many thanks and regards

Daniel

Outcomes