AnsweredAssumed Answered

Loe noise -5V source for ADA4350

Question asked by Jerry_G on Sep 18, 2015
Latest reply on Oct 5, 2015 by Andyaka

Hi, we are trying to use the ADA4350 as the first stage amplifier for the signal from a photo diode and here are my questions.

 

1. If we use +/- 5V operations, it seems the -5V source noise we have from the 7660 is very big, so what is the noise requirement on -5V source for ADA4350? And do you have any low noise -5V source chip to recommend?

2. How about if we only use 5V source for the ADA4350 operations?

3. Can I use +/- 3.3V for the ADA4350?

 

Appreciate your help very much!

 

Jerry

Outcomes