AnsweredAssumed Answered

AD9361 receiver feature

Question asked by moto on Sep 15, 2015
Latest reply on Oct 19, 2015 by tlili

Hi

 

I would like to know if AD9361 is able to receive 50MHz.

Which block limits the receiver's frequency?

UG-570 figure-5 VCO divider say, LO can set from 46.875MHz.


For example 50MHz carrier, LO set for 49MHz,..

Could you show the acceptable setting if 50MHz is ok?

The AD9361 setting will be not so many when Carrier is 50 MHz.

or Could you show us the suitable devices for 45MHz500MHz receiver?

 

Regards

moto

Outcomes