AnsweredAssumed Answered

ADIsimPLL.   What Chip model is equal to synthesizers in ADRF6720 and ADRF6850 ?

Question asked by JimPennell on Sep 14, 2015
Latest reply on Sep 14, 2015 by JimPennell

  I have need to design a system using the ADRF6720 and also the ADRF6850.   These are I/Q modulators and Demodulators with integrated VCO.

 

   However, I do not find them in the ADIsimPLL program and I want to try different loop bandwidths and so on fo rmy specific application.

 

   What Synthesizer/VCO should I choos that is the same as the ones use din these two Analog Devices components ?

 

                    Regards, Jim Pennell

Outcomes