AnsweredAssumed Answered

ADV7623: HDMI 2.0

Question asked by Mr.K on Sep 14, 2015
Latest reply on Oct 7, 2015 by JeyasudhaMuthuPerumal

Hello,

 

I am using ADV7623, ADV7612 and ADV7626.

 

I connected there devices with the HDMI2.0 Sink monitor(1920 x 1080).

The image is displayed continuously in the monitor.

However, the image sometimes becomes interrupted.

 

I think that the EDID and Rx status is correct.

I think that it can correctly read the EDID and Rx status.

Can these devices correspond to the HDMI2.0 Sink equipment?

 

Best Regards,

Mr.K

Outcomes