AnsweredAssumed Answered

ADV7623  HDCP ISSUE

Question asked by Axe on Sep 14, 2015
Latest reply on Sep 15, 2015 by JeyasudhaMuthuPerumal

Hi :

    

I have got the project file of ADV7623 from ADI team.

I have been transplanted code into the MCU of STM8S. Our sample circuit board is ready to work,

I can control switch input port via the UART port.

But there is a problem, if the input signal source with HDCP, the board will not work.

For example my signal sourc@e is BD, TV display black screen.    The attachment have a UART print information.

Should you can help me to analyze and how to support HDCP source.

Also.we  just need the fast switch function,but the code is so large.How do I quickly to remove some unwanted code for me.

Attachments

Outcomes