AnsweredAssumed Answered

ADV8005 Input and Blending Questions

Question asked by danngai on Sep 11, 2015
Latest reply on Sep 15, 2015 by JeyasudhaMuthuPerumal

Hello Video Experts,

 

1.   Can the ADV8005 take in [receive]  two separate 4K@30Hz Input Streams, perform a Blending operation, the transmit a full 4K@30Hz stream out?

 

2.   Assuming that the ADV8005 can take in two 4K@30Hz streams per above, in the Video Processor, does the ADV8005 prescale [downsample] to lower resolutions when performing a blend?  We require that the ADV8005 perform the blending function at full 4K resolution.  Chapter 3.5 of the Hardware Reference Manual seem to indicate otherwise.  Would one of the experts be able to clarify this? 

Thank you!

 

Dan

Outcomes