AnsweredAssumed Answered

ADM7154-04 max outptut volatage?

Question asked by Nole on Sep 10, 2015
Latest reply on Sep 10, 2015 by hyao

Hi all,

 

I'm building test boards for some RFIC's and considering ADM7154-04 as a power supply for 1.2V and 3.3V rails.

But, since these are test boards, I have to test IC's with power supply which varies +- 5%.

So, for +5%  of 3.3V is 3.465V. 

In the data sheet of ADM7154 is stated that maximum output voltage is 3.4V.  Is this internally limited or I could make it to produce 3.465V using external resistors?

 

I don't want to use ADM7151.

 

Regards,

Novica

Outcomes