AnsweredAssumed Answered

bug in sport driver (BF60x) ???

Question asked by pfeifferc on Sep 8, 2015
Latest reply on Nov 6, 2015 by gprasad

Hi !

first question : is there an implementation of a Talkthrough for BF60x(like the VDSP-BF537 examples.

I found a loopback example In crosscore-examples, but I need a Talkthrough -

I want to sample data from ADC and write it to the DAC with DMA via driver.

 

So I found the api function adi_sport_EnableLoopBack which seems to be working if device in receive mode.

But there is no SPORT_CTL2_LOOPBACK_EN- flag(0x00004) in SPORT_CTL2 ???

 

So this may be used in another BF-processor but not in BF60x (only 2LSB are defined in CTL2-reg)

 

kind regards chris

Outcomes