AnsweredAssumed Answered

adv7343 problem

Question asked by BarE on Sep 6, 2015
Latest reply on Sep 16, 2015 by GuenterL

hi i am using the adv7343 with fpga and adv7180 in order to transform pal to ntsc in real time. the adv7180 is part of my altera board (de2 115 cyclon 4E) and i have no problems with it. the adv7343 i bought separately and i have assembled it on my own with the tools and parts I had. I followed the circuit in the adv7343 datasheet as close as i could ,i attached the scheme with the exact values i used in my circuit.

 

מציג את 20150906_111714.jpgמציג את 20150906_111614.jpg

 

the problem i am having is with the i2c, the component is not reacting well. it gives ack when it doesn't need to give one like when i send to address 0x50 data and it doesn't give a NACKמציג את 20150906_111638.jpg

so my problem is that i don't know if the component is good or is it a problem with my circuit.

in addition i used an oscillator to generate the 27MHz freq and this is the clock:

מציג את 20150906_113428.jpg

 

the i2c writes i'm using is:

0x5600FC

0x568440

0x5682CB  \\ i am using cbvs on DAC1


thanks a lot

Attachments

Outcomes