AnsweredAssumed Answered

ADIS16137 温飘异常

Question asked by maxwell.Liu on Sep 1, 2015
Latest reply on May 5, 2016 by maxwell.Liu

我们用adis16137(1号)在做高低温测试(-40~80℃)时,发现传感器输出角度率存在较大温飘,与标称值不符合。

因为测试的时候,我们在同一个安装面上安装了另一个adis16445,两个传感器比较数据发现,温飘比16445还要大。

后来我们另外买了一个adis16137(2号),用热风枪简单的做了一个测试(27~80℃),发现温飘非常小,而同样用热风枪吹adis16137(1号),在27度时进行了自动零偏校正,然后温度升到80摄氏度,输出数据偏了0.4°/s远大于标称的±0.00125°/sec/°C。

adis16137温飘问题.png

图1、温度与Z轴输出角速率

adis16137温飘问题1.png

图2,两个传感器角速度

图2中adis16445的零偏基本符合0.005°/s/℃的标称,而16137温飘近3°/s,温变130℃左右,大于标称近20倍。

尝试过恢复初始化设置无效。

Outcomes