AnsweredAssumed Answered

ADM7171 En pin not connected to VIN

Question asked by gdownie on Aug 27, 2015
Latest reply on Aug 28, 2015 by hyao

Dear Sir/Madam,

I am using the ADM7171 in the following configuration VIN=2.5V and VOUT=1.8V.

The EN pin is not tied to VIN. The EN pin would be connected to a reset network having

a maximum voltage of +3.3V From the datasheet i can see a minimum for EN but no maximum.

Is the maximum VIN?

Regards Grant

Outcomes