AnsweredAssumed Answered

adv7511 1080p60 with ID 6

Question asked by jl-ipd on Aug 27, 2015
Latest reply on Aug 27, 2015 by mattp

Hello,

I am using a Xilinx KC705 and would like to know if the ADV7511 is able to accept as input 1080p at 60Hz with input ID 6.  I am configuring the ADV7511 with input ID 6 with 10 bits per color, YCbCr 4:2:2 DDR separate syncs, left justified.  I see in Video Input Table it mentions for this setup the maximum input clock is 82.5MHz.  I would like the FPGA to output 1080p at 60Hz to the ADV7511.  Is this possible or do I need the FPGA to output at 1080p at 30Hz to get the input clock to less than 82.5MHz?

Thank you.

Outcomes