AnsweredAssumed Answered

Issues about adv7441a with input HDMI 1080i@50HZ

Question asked by Simon on Apr 26, 2011
Latest reply on Apr 26, 2011 by DaveD

Hi

     I am using 7441 for HDMI input,and successed capture a pic with input HDMI 1080i@60HZ.but just green screem with  1080i@50HZ.

My setting is:

 

42 03 0C ; Disable TOD
42 05 06 ; Prim_Mode =0110b HDMI
42 1D 40 ; Disable TRI_LLC
42 37 00 ; Disable PCLK
42 6B E2 ; Setting cp_op_sel = 2 & Enable DE
42 68 F2 ; Auto CSC , RGB Out
42 BA A0 ; Enable HDMI and Analog in
42 C8 08 ; Digital Fine Clamp Start position
42 7B 0D ; Disable AV code Insertion
42 F4 3F ; Max Drive Strength
62 F0 10 ; ADI Recommended Write
62 F1 0F ; ADI Recommended Write
62 F4 20 ; ADI Recommended Write
6A 15 EC ; Disable these mute mask bits
6A 1C 49 ; Set MCLKOUT to output 256fs
6A 1D 04 ;  & Set Unmute Delay to 1_5 sec.
6A 5A 01 ; Reset Audio Pll

Outcomes