AnsweredAssumed Answered

Is there BF609 EZ-KIT Example code with multiple timers with seperate interrupt handlers?

Question asked by BTG Employee on Aug 25, 2015
Latest reply on Aug 27, 2015 by SachinV

I posted this question under Hardware Tools back on 8/14 with no answer (Thread 71234) so I'm hoping you can assist.

 

I'm using the BF609-EZ-KIT and I am able to get one timer to timeout and invoke an interrupt handler, but not two or more.. I’m using the adi_tmr_Open and associated driver utilities that came with the kit.  The datasheet seems to indicate that there are up to 8 timer interrupts that can be used.

 

Do  you have some example code with multiple timers each invoking their own interrupt handlers upon timeout?

 

I have not found an example with more than one timer interrupt handler in the kit.

Outcomes