AnsweredAssumed Answered

Fmcomms3 with Zynq ZC702

Question asked by ThomasL on Aug 24, 2015
Latest reply on Aug 25, 2015 by KE5FX

I just get two Fmcomms3 and I use them with the Zynq ZC702.

I've try the quick start guide but I didn't get anything on the IIO scope. As you can see on the following picture there is an error with the SPI bus and the clock when I boot on the SD card with the UART terminal.

In the IIO scope the only device that I've found is an xadc.

Do you have an idea? Is there something to do to synchronize the daughterboard and the motherboard?

 

fcommsError-2.JPG

Outcomes