AnsweredAssumed Answered

DC offset changing or aliasing?

Question asked by Daniel_Camara on Aug 24, 2015
Latest reply on Aug 31, 2015 by larsc

Hi people,

 

  I know you are not there to teach me signal processing, even though you have done quite some times . I wan to know if you have any ideas the why of this behavior (see image). I am not sure it is the DC offset, or some sort of aliasing the thing is that it also happens when I use the  BIST on the TX, but it is less perceptible, see detail in figure 2 (Pay attention that the graph is with 10000 samples, just to make the phenomena clearer). The image below, figure1, is the packet I generated, and you can see the effect is strange. As the DC offset  is set to auto I hoped it would have an envelop more or less constant.  Could be a problem of sampling or of a "loose" harmonic, but I set the RF bandwidth to the minimum 1MHz and I had no perceptible change.  The TX and RX sampling rates are also the same..  Any ideas?

 

The main parameters:

FDD,

Calibration mode: auto

RX/TX RF Bandwidth: 1MHz

RX/TX Sampling rate: 8MSPS

RX/TX LO Frequency: 2.4GHz

RX gain: fast_attack/Manual gain 5

TX attenuation:0

Cable between TX board 1 and RX board 2

 

  Any ideas why the I/Q vary this way?

 

 

Outcomes