AnsweredAssumed Answered

ADM3485's differential input threshold voltage vs input frequency

Question asked by moto on Aug 24, 2015
Latest reply on Aug 25, 2015 by moto

Hi

I would like to know about the Differential input threshold voltage of RS-485 receiver.

It should be -0.2V/+0.2V

 

Does it depend on the signal frequency?

 

I checked ADM3485 by 5MHz square wave, then it needs over 0.8V amplitude.

(When it inputs the sine wave, then it needs over 1V amplitude)

The duty is 50%.

At 200KHz, the threshold is about +/- 0.2V.

 

Does this feature meet the RS485 specifications?

 

The input level will change the delay time?

 

How to measure this threshold?

 

Could I have the advice?

 

 

Regards

moto

Outcomes