AnsweredAssumed Answered

MATLAB loading DPG3 to drive AD9152

Question asked by mike.ericson on Aug 21, 2015
Latest reply on Sep 1, 2015 by Biao.H

Hello,

 

I found these command in a sample MATLAB script to load the DPG3 (or DPG2 in this case):

 

dpg_array = NET.convertArray(original_array, 'System.Int32');

dpg2.DownloadInterleavedVectorInt1D(dpg_array,2,true);

 

However, that format does not seem to be correct for the AD9152-ADRF6720 evaluation board that I have.  What are the equivalent commands for the AD9152?  I've done some experimentation but, if someone there knows, I'd welcome the help.

 

The board works as expected when using the DPG Downloader GUI, but I'd like to automate the testing with MATLAB.

 

Thanks very much,

Mike

Outcomes