AnsweredAssumed Answered

How do I sync 2 or more ADA2200?

Question asked by jwdossey4604att@yahoo.com on Aug 14, 2015
Latest reply on Aug 17, 2015 by Gustavo.Castro

I would like to connect more than 2 ADA2200s together to sense voltages on a physical system.  They all run from the same external 10MHz system clock. I want to use high frquency divider /16, decimator /8, and RCLK /8.  How do I make sure all ADA2200s start at the same time so all the RCLKs are in sync?  Or is there a way to sync RCLKs from the several ADA2200s?

Outcomes