AnsweredAssumed Answered

AD605 self excited

Question asked by shafa on Aug 12, 2015
Latest reply on Aug 17, 2015 by shafa

We are now trying to build a multi-channel ultra-sonar receiving system. For the sake of power consumption and budget consideration, each 8 channels are multiplexed into one after the band pass stage; as a result, the whole 384 channel data can be sampled by 48 16-bit ADCs. The BP has a central frequency of 300kHz and a band width of about 30kHz.

 

Since we need a dynamic range of 96dB, we are using AD605 for the VGA stage. By default AD605 receives a differential input and gives a single end output, but we use single end mode for both input and output, because it says OK in the datasheet.

The problem we are facing is that the chips (AD605) we are testing are easy to get self excited, when VGN exceeds 2V. It looks like as VGN goes higher, the output signal is modulated by a high frequency (about 13~19MkHz), and if VGN is higher enough, there is a very high frequency output, even when no input signal is applied. This is hard to explain. Cans some help?

(some figures are included in the attched docx for better illustrating)

Attachments

Outcomes