AnsweredAssumed Answered

Can I hack ADP2140 to produce a different voltage on the switching output?

Question asked by Dorin on Aug 11, 2015
Latest reply on Aug 12, 2015 by Dorin

Hello everybody

I have a legacy design in which 3.3V and 1.8V are produced using the ADP2140ACPZ3318.

There are no available parts on available at any distributor.

 

I was thinking to use the 2.5/1.8 or the 1.2/1.8V versions which are available,

and force the switching supply to produce 3.3V by inserting a resistor in the feedback path

(between FB pin and inductor as in Fig.1 of the datasheet).

 

Could you recommend me the value of the resistor to use

Alternatively, I would appreciate to if someone could reply with the input impedance or the bias current on the FB pin.

 

Sincerely

Dorin Calbaza

Outcomes