AnsweredAssumed Answered

AD8134 Help Required

Question asked by Arsi491 on Aug 10, 2015
Latest reply on Aug 26, 2015 by Arsi491

Hello everyone,

 

I require to convert RGsB (Gs means "Sync on Green") signals of a Single Ended video stream into Differential output.

I researched and found AD8134 to be suitable for the job. I developed an evaluation board on the resources available on Analog Site, and I looked at following discussion to create a board for AD8134 (I used the designs for AD8142 (same as AD8134) in the answer of AnnaFeB ):

 

https://ez.analog.com/message/211413#211413

 

 

However, in my card i kept the option to give a "negative 5" volt supply. In my case, i have no use for Vsync, Hsync and Sync Level pins (atleast that is what i think, since my Sync signal is on GREEN line), so there fore i have left these three signals "DISCONNECTED"

 

My issue is that once i start the board, power it up at "Positive and Negative 5 volts", and give no input, i get strange results on my outputs. the Red outputs, show no value, the green outputs show "negative 1 volt", while the blue output shows "Positive one volt". When i give an Input signal of "+1 volt" at all 3 positive inputs ( the negative inputs are grounded), i receive following outputs:

 

    1) R+ and R- show nothing

    2) G+= -1, G- = -2

    3) B+= +2, B-= +1

 

I do not think this working correctly, does this have something to do with the three signals i left unconnected?  please help..

Outcomes