AnsweredAssumed Answered

Supply Voltage of AD8137

Question asked by christian.h on Aug 10, 2015
Latest reply on Aug 10, 2015 by harryh

Hi,

 

The operating voltage of the AD8137 is specified as 12V max in the datasheet. This is also the voltage at which we operate it. Looking again into the datasheet, I found that this is identical to the absolute maximum rating. This might be exceeded in our circuit by 170mV due to tolerances in the voltage supply.

Now I am concerned if we should modify the PCBs in order to meet the maximum rating. This would mean some effort, because the PCBs are already installed in a setup.

Any recommendations?

 

Best Regards,

Christian

Outcomes