BrettG

Peak Full Range Compressor

Discussion created by BrettG on Apr 21, 2011

The Peak Full Range Compressor was accidentally included in the libraries for the AD1940 and ADAU1701 cores. However, the code contains instructions that cannot be executed on those cores. Therefore, a compiler error will occur if these cells are included in a project.

 

ScreenHunter_02 Apr. 20 18.44.jpg

 

The next release of SigmaStudio will remove this cell from the AD1940 and ADAU1701 libraries, instead only including it in the ADAU144x, ADAU1761, and ADAU1781 libraries.

Outcomes