AnsweredAssumed Answered

GNU radio program  error  for SDR  AD9361 FMCOMMS3  kit  Z706

Question asked by calltogaurav on Aug 5, 2015
Latest reply on Aug 24, 2015 by calltogaurav

while running example programme FM receiver on SDR kit based on Z706 and FMCOMMS3  following error occurred

20150723_153907.jpgi  could solve

i could solve one error of "failed to enable real time scheduling " by running GRC in root

but others error i.e. "unable to create temp file :22 " persist

in this forum solution is given for zedboard but not for Z706 based FMCOMMS3  kit

at present i am using latest SDK image released on Apr 24 ,2015 ,which include inbuilt support for GNU Radio

Outcomes