AnsweredAssumed Answered

A non-recoverable error or exception has occurred

Question asked by pfeifferc on Aug 4, 2015
Latest reply on Sep 21, 2015 by StuartS

On our new BF607 based board i get the following error

A non-recoverable error or exception has occurred.

   Description:  A data CPLB miss has occurred without a corresponding CPLB entry. 

   General Type:  RunTimeError   Specific Type: DCPLBMissWithoutReplacement

   Error PC:      0xffa019b0

 

I have 2test programms loaded into each core of the BF607.

DDR2 Memory is configured within Corsscore and Mem at 0x0 is working in IDE

but if i use a Memory derived from Power_On_self_test for EZKitBF609 the CPU based memtest fail with this errormessage.

DMA based test is working.

So i write a simple external Mem test like

pInt=0; //ptr to ext. mem

*pInt=12;

--- error is the same - is there any missing configuration of any Register or in the Project ????

 

Kind regards chris

Outcomes