AnsweredAssumed Answered

Implementation of User IP in Reference Design for Zedboard and FMCOMMS2

Question asked by Chris90 on Aug 4, 2015
Latest reply on Aug 4, 2015 by CsomI

Hi,

 

for my final work of my studies I should implement my developed transceiver IP Core in the Reference Design of Analog Devices. I am using the Zedboard and the FMCOMMS2.

 

In the figure below I am showing my thoughts how to implement my IP Core in the Reference Design. I am not sure if it is correct because during the test I recognized that the DAC_enable signals are low-active. How is it possible to set the dac_enable high-active? Furthermore, I am not sure if it is correct to insert my own IP during the axi_ad9361_dac_dma and the util_dac_unpack. Is it also possible to neglect the dac_unpack because the output of my IP core are also I-Q data.

 

For the receiving part I am thinking to implement my IP Core between util_adc_pack and axi_ad9361_adc_dma. Would it be also possible to neglect the adc_pack core?

 

Thank you,

Christian

Attachments

Outcomes