AnsweredAssumed Answered

ADP1614; Largest SS capacitor allowed?

Question asked by drfriedparts on Jul 28, 2015
Latest reply on Jul 29, 2015 by hyao

What is the largest capacitor that can be used on the Soft Start pin of the ADP1614? It contains an internal low-side switch to reset the capacitor in response to certain events (such as thermal shutdown) which implies that there is an upper board on the size of the soft-start capacitor, but the datasheet is silent. I'm looking to use a very long soft start time (~250ms), which, in turn, requires a 1uF cap or so.

Outcomes