AnsweredAssumed Answered

HMC586

Question asked by ADIguy on Jul 23, 2015
Latest reply on Jul 30, 2015 by MRichardson

Hello,

 

The absolute max tune voltage for the HMC586 is shown as 0 to 22 volts, with the normal operating range as 0 to 18V. Can Vtune be applied to the device before the +5 VDC? I also wanted to check if there are any concerns if the input clamp allowed a -0.3 V on the Vtune input?  Could this cause an issue such as latchup when the input returns to the normal range?

 

Thanks and Best Regards.

Outcomes