AnsweredAssumed Answered

ADI_FMCOMMS2 DTSI FILE

Question asked by hplee on Jul 23, 2015
Latest reply on Jul 31, 2015 by mhennerich

Hi,

My customer has built the kernel Linux for MicroBlaze with modified adi_fmcomms2.dtsi file of 30.72MHz reference clock

(original adi_fmcomms2.dtsi file of 40MHz reference clock).

 

They have followed the instructions exactly as below link.

  http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/linux/microblaze

 

The log file of original kernel is log_kernel.txt. 

 

The log file modified kernel is log_kernel_rebuild.txt

But, the result is not correct.

 

The log_kernel_rebuild.txt file has line 37&38: /amba_pl/ which is not same as log_kernel.txt has line 38&39: /axi@0/

 

Do you have any idea where it goes wrong?

 

Attachment for log files.

 

Please advise...

 

 

Thank you.

 

 

 

Attachments

Outcomes