AnsweredAssumed Answered

AD9129 eval brd interface speed

Question asked by HankZ on Jul 21, 2015
Latest reply on Jul 22, 2015 by rejeesh

We are looking into using an AD9129 in a new design.  Your eval board (with the Xilinx ML605) is stated to run at 2400 MHz, with the Virtex-6 DDS core running at Fdac/3 (800MHz).  According to the Xilinx data sheet, the maximum frequency the DDS core can run at is 452 MHz in the even-more-advanced Virtex-7.  Can you explain how you are able to get this performance? Any guidance you could provide on running the AD9129 at 2400 MHz would be GREATLY appreciated.

Outcomes