AnsweredAssumed Answered

What is the output current of ADP3335 MSOP ?

Question asked by elsalvador on Jul 20, 2015
Latest reply on Jul 28, 2015 by jespirit

Dear sir.

What is the maximum output current of ADP3335ARMZ-3.3-RL(MSOP) ?

Even theoretical maximum current of ADP3335 MSOP is 300mA.

As I checked, it just can be maximum 100mA.

 

Its condition is below.

Input voltage is 5V

Output voltage is 3.3V

Ambient temperature is 35 Cels. degree.

Outcomes