AnsweredAssumed Answered

AD8436 - DC Current measuring

Question asked by bskhoo on Jul 19, 2015
Latest reply on Jul 20, 2015 by jstaley

Hi all,

 

Need your advice, if AD8436 can be use to measure DC current for 3.3V, 5V and 12V.

 

Attached is the block diagram.

 

1) To measure the current going into DUT(Device Under Test)

2) A shunt resistor is place between IBUFIN- and IBUFIN+

3) The output from IBUFOUT is connected directly into RMS (without cap) since it's a DC voltage.

4) OUT to connect to customer MCU to measure the current.

 

Thks

 

Regards,

  BS Khoo

Attachments

Outcomes