AnsweredAssumed Answered

Using UART2 vs UART0 with FREERTOS

Question asked by CIMSOR on Jul 17, 2015
Latest reply on Aug 26, 2015 by gvasanth

My project requires the use of UART2 (TX only) within the FREERTOS environment. I started with the FREERTOS UartCharEcho example. Very simple modifications while using UART0 work as expected. However when UART2 is selected, the program hangs at adi_uart_Write (line 274). The adi_pinmux.c was changed to allow UART2_TX. UartCharEcho was modified only to change Uart parameters and can easily be switched to UART0 or UART2 via define selection near top. Suggestions appreciated.

Thanks,

Bob

Attachments

Outcomes