AnsweredAssumed Answered

ADV7612 in a smaller package?

Question asked by brendan on Jul 15, 2015
Latest reply on Jul 16, 2015 by brendan

I am currently using the ADV7611 for my product, but am finding it doesn't support the full range of HDCP products (such as PS3, Chromecast, Galaxy S4).  It looks like the ADV7612 will support a larger range of product, but it is too large at 16.2mm square to fit on my PCB and would entail a full redesign of the PCB and outer housing.  My questions are:

 

1. Do you have a product that supports a larger range of HDCP products but in a smaller package like the ADV7611 (12.2mm square),

 

OR

 

2. can the ADV7611 be configured differently to run a larger range of HDCP product?

 

Thank you!

Outcomes