AnsweredAssumed Answered

What are the required ADV7604 Register settings for DVI-A at1920x1200, F/R=50 & 30?

Question asked by BTG Employee on Jul 14, 2015
Latest reply on Jul 23, 2015 by DominicB

Hi,

 

A colleague tried posting was having trouble so I'm posting again.

 

Referring to: ADV7604 Component/Graphics Digitizer with 4:1 Multiplexed HDMI Receiver Hardware Manual Rev. F August 2010.

 

We are trying to do DVI-A (Analog DVI) at 1920x1200 with frame rates of 50 and 30.   There is no PRIM_MODE[3:0]  or VID_STD[5:0] setting listed in Table 3: Primary Mode and Video Standard Selection nor for the V_FREQ[2:0], IO Map, Address 0x01, [6:4] setting in Table 4: V_FREQ[2:0] Description.

 

What are the complete register settings we need to make to get DVI-A (Analog DVI) at 1920x1200 with frame rates of 50 and 30.

Outcomes