AnsweredAssumed Answered

AD9361 eval board support software

Question asked by RFRM on Jul 14, 2015
Latest reply on Jul 14, 2015 by pcercuei

I've set up the AD9361 eval board FMCOMMS2-EBZ with the ZYNQ ZC706, it works fine with the on board Linux IIO oscilloscope.

 

I note that at IIO Oscilloscope [Analog Devices Wiki] that at Windows application is mentioned, and a file available to download to allow However, there does not appear to be any further information and when I run the application on an XP machine I get an Entry Point not found error (The procedure entry point inet_ntop could not be located in the dll WS2_32.dll)

 

What I was wanting to do was to connect the ZYNQ ZC706/AD9361 eval board combination via Ethernet to a remote laptop so that I could run IIO Oscilloscope on the laptop - as I said, I can't see any further information on the Windows app. Is there any more information anywhere ?

 

Rog

Outcomes