AnsweredAssumed Answered

AD8000 output distortion

Question asked by sbandara on Jul 8, 2015
Latest reply on Jul 23, 2015 by sbandara

My circuit simulation working perfectly on the simulation. But in the real world, it would destroy the input signal and also output completely

requrement

input 100 mV peak-peak

frequency-50Mhz

Gain is about 40 to 50

slew rate is about 1580 V/µs

 

I did not construct the circuit on the PCB. Instead of that I did on the “breadboard”

When I was input pure sine wave by the signal generator it destroyed the input signal shape and output signal shape

 

I am attached here with multisim circuit diagram and the similar image of the output distortion

(I did not take the photo of the oscilloscope output)

Attachments

Outcomes