AnsweredAssumed Answered

Looking for a SPDT switch to select between two negative AC signals

Question asked by jkl on Jul 6, 2015
Latest reply on Jul 9, 2015 by KRZ

I have two AC signals (0V to -75V) and would like to use a SPDT switch to select between the two signals. The resulting signal drives a 30pF piezo that requires less than 1mA of current. The input frequency is a relatively slow rate of less than 1KHz. Has anyone had to deal with this type of application, and have any ideas on implementations?

Outcomes