AnsweredAssumed Answered

drive AD9838 with low p-p clock

Question asked by H.Alagi on Jul 6, 2015
Latest reply on Jul 7, 2015 by H.Alagi

Hi everybody,

 

Is it possible to drive the AD9838 (supply voltage 5 V) with an oscillator (X1G0041710011 SG-210STF 5 MHZ L, supply voltage 2.5 V)?

The output Voltage of the oscillator is about:

V_OH 90% Vcc Min

V_OL 10% Vcc Max

 

Dose the Parameter LOGIC INPUTS of the AD9838 describe the clock-input characteristic?

 

Best regards

Hosam

Outcomes