AnsweredAssumed Answered

HMC253QS24E Pin spec

Question asked by mst20xx on Jul 6, 2015
Latest reply on Jul 13, 2015 by mst20xx

I have some questions about HMC253QS24E .

 

1) Absolute Maximum Ratings

According to datasheet , Maximum Input Power +20 dBm (0.05 - 0.5 GHz)

+24 dBm (0.5 - 2.5 GHz) .

Is  it same spec for all pin (RFC and RF1 to RF8 ) ?

 

2) When RF1 to RF8 are input pins and RFC is output pin,

How many ports can use hot switch ?

 

3) What is max input power when switch ON/OFF during RF1 to RF8 are input signal at the same time ?

(Example +20dBm/Port × 8Ports = +29dBm / Total??)

Outcomes