AnsweredAssumed Answered

USB and UART on BF527

Question asked by Sean2011 on Apr 8, 2011
Latest reply on Apr 25, 2011 by CraigG

Hi,

I'm attempting to use the examples provided for the BF527 to create an application which uses both USB and UART on a Blutechnix BF527 module. The examples in question are Blackfin\Examples\ADSP-BF527 EZ-KIT Lite\Drivers\UART\Autobaud and Blackfin\Examples\ADSP-BF527 EZ-KIT Lite\Drivers\usb\bulk_loopback_app.

 

I'm try to add USB functionality to the UART Autoband example. I've added the neccessary headers and variables, and enabled external SDRAM. I then try and initiliase the USB in the adi_ssl_Init() function. However the program immediately jumps to __unknown_exception_occured when run if any code to set up the USB controller (like adi_usb_CoreInit((void*)&Result); ) is included in the ssl init routine.

 

In what order should I initiliase the devices? What's the best approach for doing this?

 

Any help/advice would be appreciated.

Outcomes