AnsweredAssumed Answered

SPIH speed?

Question asked by amf on Jul 3, 2015
Latest reply on Jul 22, 2015 by emoloney

In various places, the documentation claims that SPIH port can transfer data at a max rate of 8 MHz, 12 MHz or 16 MHz.  Which is correct?  Attached are screenshots showing the posted FAQ says 16 MHz.  However, the SpiFlashTest example says 7,999,999 Hz. 

 

Also, I think there's another typo in the FAQ.  The SPIH is connected to the AMBA bus, not the APB bus, correct?

Outcomes