AnsweredAssumed Answered

EVAL01-HMC877LC3

Question asked by ShulabhGupta on Jul 2, 2015
Latest reply on Mar 12, 2016 by congnt2506

Hi,

 

I am trying to reproduce the application note results (phase shifts and S-parameters) for a brand new evaluation board of HMC887-LC3. I am however unable to get those results for single-ended operation (desired). Here is the board configuration I got:

 

LC ~3.5V

VCC = 3.3 V

0DWN = GND

VAC ~1.7 V

VDCN = VCC = 3.3 V

VDCP = [2.7 V - 3.3 V]

INP = port 1 of the VNA

QP = port 2 of the VNA

INN= DC Block + 50 ohms

QN = DC Block + 50 ohms

Remaining terminals = GND

 

I want to vary the S21 phase shift as a function of VDCP, over a bandwidth of 10-20 GHz. Can someone please assist in debugging the issue?

 

Thanks.

 

..Shulabh

Outcomes