AnsweredAssumed Answered

ADXL103/ADXL203

Question asked by mark.allie on Jul 2, 2015
Latest reply on Jul 3, 2015 by neilzhao

I was wondering if anyone knows if one can leave an output pin completely open if you don't need the output signal. I understand that there will be a lot of clock noise on it. The data sheet almost threatens the worlds end if you don't put at 1nF or larger ;-) on the output pin. I assume this is for S/N reasons and not anything inherent in the part functionality. This question is because I want to put a 203 on a board designed for a 103 and the Y axis output pin is unconnected. Perhaps a 5g full scale 103 could be made?

Outcomes