AnsweredAssumed Answered

ADV7611 Reset

Question asked by joerg Employee on Jul 2, 2015
Latest reply on Jul 2, 2015 by mattp

On some systems with the ADV7611, where the RESET is pulled down by a 10k
resistor, the level at the Pin still is at 1.5V.

Therefore Reset is not executed and the crystal does not start up.

Questions:

- could you provide a block-diagram of the internal circuit of the RESET Pin?

- Is the I2C interface working if the crystal does not start up? And if it started and stop again is it then still working (like it is on the ADV7180?)

Outcomes