AnsweredAssumed Answered

twi problem with BF60x and AR0130 sensor

Question asked by jihen on Jun 29, 2015
Latest reply on Aug 31, 2015 by SachinV

Hi,

 

I am trying to connect An AR0130 demo sensor board to an ADSP-BF609_Ezikit board.

I tried to use the "VideoLoopbackRGB" project which is under "Camera_EI3_Extender_Board-Rel1.1.0\Camera_EI3\Blackfin\Examples\ADSP-BF609\MT9M114".

 

I changed the registers and all needed things according to AR0130 sensor  datasheet.

I have a configuration :

In first call of "adi_twi_Write" function, "drv->pData->buffer1.bError = 1", whereus the result of "adi_twi_Enable" is "ADI_TWI_SUCCESS".

 

Do you have any suggestion?

 

Thanks

Outcomes