AnsweredAssumed Answered

ADIS16448 default register values differ from datasheet

Question asked by Heino on Jun 24, 2015
Latest reply on Jun 24, 2015 by NevadaMark

When I readout out all of the ADIS16448 registers, some values are different then expected w.r.t. the datasheet. The register update sample rate was very slow (each 2.5s). After some research I found this was due to the value of register 0x36 (SMPL_PRD). This value should be 0x0001. In my case the value was 0x0B01. The value of D, decimation rate setting was 11 instead of 0. 11 indeed corresponds with an update rate of 2.5s.

 

Is this a known issue that the default values are sometimes different then mentioned in the datasheet?

In the attachment a screenshot of al the default register values after power-up.screenshot default reg values ADIS16448.JPG

Outcomes