AnsweredAssumed Answered

JTAG connector options

Question asked by ChristianH on Jun 24, 2015
Latest reply on Jun 29, 2015 by ChristianH

Hi,

 

normally we are using the HPUSB-ICE emulator for debugging SHARC DSPs together with VisualDSP++.

On a new PCB we have some size limitations. I'm wondering if I could use a smaller connector on the target board.

 

I'm thinking of making an adapter cable or board from the 14pin connector on the HPUSB-ICE cable to a small connector (8/10pins, SMT).

I've seen through the EE-68 but found no final answer on limitations or considerations when going that way.

 

The ICE-1000 has a smaller (still not really small) connector using 10 pins (J2 connector).

But the ICE-1000 is mechanical to big to be able to connect to a target board connector.

 

Any ideas or tips for me?

 

Regards

Christan

Outcomes